Post Go back to editing

LTC2357-16 keeps shorting 5 volt rail to ground.

Category: Hardware
Product Number: LTC2357

I'm stuck in a strange scenario here. I have a board made based on a 6 page Schematic that works ok until I add the LTC2357. At which point the LTC2357 shorts my 5 volt rail to ground pulling 200mA ( showing 1 ohm from ground to 5v). Removing the chips clears the short and with the chip out the 5v input is in fact shorted to ground. At first I thought maybe it was ESD or other mishandling so I just replaced the chip. This corrected the  issue and the ADC worked but I noticed other components like one of the OP  AMPs stopped working. In fixing the OP amp, the ADC became shorted again. Seems maybe two chips are playing tug-a-war or maybe I'm soldering at too high a temp, or some other bad practice. At the cost of these chips I need to figure out my game plan. 

I need to know these answers if anyone can help. And please, if anyone has a thought, do suggest.

1) Does anyone see anything wrong with this Schematic below? I can add others if need be but think it has to do with these two.

2) The supply voltage to the board is +15,  -15, and 3.3. I add them in this order. Ground, +3.3, +15, +15. To remove them I remove all 3 power sources at once, then ground.  Is this causing my issue?

(note) the Schematic does indicate +/- 12 but we are currently using 15. I do not see any issues with this that stand out.

3)  I solder at 810f



Moved & added tag.
[edited by: emassa at 2:04 PM (GMT -4) on 28 Jun 2023]