Post Go back to editing

AD4115 GPIO Input levels

Thread Summary

The user inquired about the AD4115 ADC's GPIO input voltage levels, noting a discrepancy in the datasheet regarding 3.3V support. The final answer confirmed that the AD4115 does not support 3V operation and directed the user to an FAQ for the GPIO input voltage thresholds. The user later confirmed that the GPIO inputs can be used with 3.3V logic levels.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD4115

Hello,

An other question about this ADC and the two available GPIOs that can be used as inputs.

I was surprised that the GPIOs are related to analog voltages (wrongfully said to be usable to 3.3V on page 36, which was one of the reasons why we choose this ADC and had to add a 5V line at the last moment..), but there is no information about the characteristics of these lines. We can not use the outputs as we don't have any 5V logic, but perhaps there is a hope to be able to use thee inputs with 3.3V levels.

But the datasheet does not tell what are the low/high levels or these.

Anybody knows or have checked ?

Thanks in advance,

Jerome.

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.