Post Go back to editing

AD7980 in 4-WIRE CS MODE WITHOUT BUSY INDICATOR, How many AD7980 can be conected in this way? In datasheet, the example of this application is only two parts, if possible, connected three or more?

Thread Summary

The user encountered issues when connecting three AD7980 ADCs in 4-WIRE CS mode without a busy indicator, observing conflicts on the SDO lines. The solution involves ensuring that only one CS is low at a time, and the user should verify the timing of CS transitions. The user also noted that the SDO lines did not revert to high impedance immediately after the SDI was pulled high, which could be a contributing factor.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD7980

AD7980 in 4-WIRE CS MODE WITHOUT BUSY INDICATOR, How many AD7980 can be conected in this way? In datasheet, the example of this application is only two parts, if  possible,  connected  three or more?

Edit Notes

update the issue. PN is AD7980
[edited by: Sara123 at 8:11 AM (GMT -4) on 16 Jun 2023]
Parents Reply
  • It seems that there is a problem with my English, which has been the problem since the beginning. Three SDOs connected together have been unable to function properly. To find the reason, I separated the SDO and discovered a conflict. I want to see if anyone can prove me wrong. Find examples of three AD7980 SDO connections working properly together.

    From the beginning until now, the problem has always existed. There has been no progress.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.