Post Go back to editing

AD7980 in 4-WIRE CS MODE WITHOUT BUSY INDICATOR, How many AD7980 can be conected in this way? In datasheet, the example of this application is only two parts, if possible, connected three or more?

Thread Summary

The user encountered issues when connecting three AD7980 ADCs in 4-WIRE CS mode without a busy indicator, observing conflicts on the SDO lines. The solution involves ensuring that only one CS is low at a time, and the user should verify the timing of CS transitions. The user also noted that the SDO lines did not revert to high impedance immediately after the SDI was pulled high, which could be a contributing factor.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD7980

AD7980 in 4-WIRE CS MODE WITHOUT BUSY INDICATOR, How many AD7980 can be conected in this way? In datasheet, the example of this application is only two parts, if  possible,  connected  three or more?

Edit Notes

update the issue. PN is AD7980
[edited by: Sara123 at 8:11 AM (GMT -4) on 16 Jun 2023]
Parents Reply
  • In 3 AD7980 systems, when AD7980A completes sending data, the SDOs of AD7980B and AD7980C will output data at the same time, which may cause conflicts. But in 2 AD7980 systems, when AD7980A completes sending data, only AD7980B is waiting. There are no problem with the 2 AD7980 systems. I don't know what I can do?

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.