MAX22530AWE+ have Vref output (REF, 1.8V) and VDDF (higher, ex 3.1V). May I use this outputs to supply very low current external load like TSC210 (current op-amp from ST, it use Vref and VCC - so VDDF to VCC, Vref to REF)
MAX22530
Recommended for New Designs
The MAX22530–MAX22532 are galvanically isolated, 4-channel, multiplexed, 12-bit, analog-to-digital converters (ADC) in the MAXSafe™ family product...
Datasheet
MAX22530 on Analog.com
MAX22530AWE+ have Vref output (REF, 1.8V) and VDDF (higher, ex 3.1V). May I use this outputs to supply very low current external load like TSC210 (current op-amp from ST, it use Vref and VCC - so VDDF to VCC, Vref to REF)
quiescent current of TSC210 is about 0.1mA, output will be connected to the input of MAX22530AWE+
Hi pinelab ,
Only Maxim ATE products are supported on EngineerZone at this time. Over the next several months, you will see more Maxim products being supported in EngineerZone. Please visit one of the technical support pages on our newly integrated website below for assistance with Maxim Integrated products.
EN - https://www.analog.com/en/support/technical-support.html#
CN - https://support.analog.com/zh-CN/technical-support/
JP - https://support.analog.com/ja-JP/technical-support/
Regards,
JC
Hi JCCillion, is MAX22530AWE+ not a "Maxim ATE" product?