LTC2380-24
Production
The LTC2380-24 is a low noise, low power, high speed 24-bit successive approximation register (SAR) ADC with an integrated digital averaging filter. Operating...
Datasheet
LTC2380-24 on Analog.com
hello.
I am testing dc2289a-a with dc590b.
Currently, the highest sampling rate is 1 ms as confirmed by an oscilloscope.
I want to increase this to the maximum sampling rate of the ltc2380-24 adc. What should I do?
The DC590 cannot be used to set sample rates. Use DC890 to run DC2289A at it's full sample rate.
The DC590 cannot be used to set sample rates. Use DC890 to run DC2289A at it's full sample rate.
Thank you for answer. I'll have to think of another way.