LTC2380-24
Production
The LTC2380-24 is a low noise, low power, high speed 24-bit successive approximation register (SAR) ADC with an integrated digital averaging filter. Operating...
Datasheet
LTC2380-24 on Analog.com
hello.
I am testing dc2289a-a with dc590b.
Currently, the highest sampling rate is 1 ms as confirmed by an oscilloscope.
I want to increase this to the maximum sampling rate of the ltc2380-24 adc. What should I do?
The DC590 cannot be used to set sample rates. Use DC890 to run DC2289A at it's full sample rate.
Thank you for answer. I'll have to think of another way.