Post Go back to editing

MAX22531 input protection (overvoltage, reverse polarity)

Category: Hardware
Product Number: MAX22531

Hello,

currently, we're designing a layout using the MAX22531 isolated ADC.

For that, the maximum 400V AIN_ input on the secondary isolated side is regulated down to the maximum 1.8V Vref of the internal reference of the ADC.

To protect against overvoltage, I though a voltage clamping circuit with zener diodes might work. However, R52 has to be very large to limit current flow in the ADC which may be a problem.

Can someone point me out the correct way to have both overvoltage and reverse voltage protection?

Do I need R52, when I'm adding a fuse between Z2 and GNDA, or will the ADC be damaged before it is triggered?

Thank you!

Best,

Andy

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.