Post Go back to editing

In AD7150 capacitance value is showing negative value?

Category: Hardware

In AD7150 capacitance values is increasing and suddenly it starts to decrease and show negative value. What could be the reason behind it?

  • Hi  ,

    We will look into this. I will contact the product owner and get back to you.

    Regards,

    JC

  • Hi rrk1812,

    With the provided information we cannot know what is going on. Could it be that the capacitor values is out of range?

    Could you provide more information about the Measurment procedure?

    Regards 

  • Dear Joan0rtega

    Basically, my application is on sensors for humidity measurement. I have 4 copper electrodes, of which two electrodes (C and D) are grounded.

    The electrodes A and B are connected to the Cin and Exc pins of the board to measure the capacitance between these two electrodes.

    I am using paper with a nanoporous coating as a substrate.

    When the relative humidity increases the relative permittivity increases and thus the capacitance increases.

    The capacitance is showing an increasing change with increasing RH but after a certain point the capacitance value suddenly starts dropping (although it is in the range and I am using 2pF as input capacitance range) and it settles to a negative value (image attached).

    I do not know what this negative value is indicating.

    Please help with the same.

    Thanks

  • Hi rrk1812,

    I cannot tell what is going on but could you provide me the current configuration of the CDC to check if I see anything in the configuration?

    It seems like it is saturating to 0.71pF.

    What is the value of the CAPDAC?

    Regards

    Joan

  • Sir the CapDac value is zero throughout.

    The sensor has 4 electrodes where 2 of which are connected to Cin and Exc that is electrodes A and C (its capacitance is to be noted down) and the remaining terminals are grounded.

    The gap between the electrodes is 1 mm (the black space between the electrodes) and the electrode material is copper.

    the substrate material is PCB with FR4 

  • Sorry rrk1812, but the sensor design is out of my expertise.

    I can support you with the schematic design and with the configuration of the device but unfortunately if the problems is with the sensor I cannot help you.

    If you send me the register configuration and the schematic I can check if there is something wrong..

    Regards

    Joan