According to the data sheet, the Sinad and snr are supposed to be close to 70db or 69db for even 100KHz frequency of input signal. But actually when I am giving the signal using analog discovery 14 bit input source wavegen function, it gives SNr of 63db which is not even close. Can u please state the reasons. I have also connected a RC filter at R83= 160ohms and C121= 10nF . But still snr is around 63dm . Please help me in this regard.