Post Go back to editing

AD2S1210 set Encoder resolution!

Category: Hardware
Product Number: AD2S

I use AD2S1210. Everything's fine. But when I set the Control Logger (0x92) to change the resolution of the Encoder, I only get the 10bit encoder output, while the resolution of the position read is settable by Res1 , res0. I read (0x92) that D2 and D3 are already set. what's going on with AD2S1210?
Look forward to the help

Parents
  • Hi  ,

           I wanted to understand your current set up. In your set up, what is the setting of D2 and D3? You mentioned that is only 10-bit encoder, how many pulses are there in 1 revolution? As discussed in the Incremental encoder section of the datasheet, a 12bit resolution will have 1024 pulses in A and B. A lead B by 90degrees. Each A and B cycles will have 4 counts. 1024 pulses will have 4096 counts which is a 12-bit resolution. 

    Regards,

    Jonathan

  • Thank for your reply!

    I have encoder reader. I understand you want to talk: 10 bit- A cycles =256ppr, 12bit- cycles =1024...

    When i set Res0=1, Res1=1, then Position data that I read is exactly 16 bits. 

    But i change D2 and D3, then the value of A cycles  remains constant 256ppr, it doesn't change

Reply
  • Thank for your reply!

    I have encoder reader. I understand you want to talk: 10 bit- A cycles =256ppr, 12bit- cycles =1024...

    When i set Res0=1, Res1=1, then Position data that I read is exactly 16 bits. 

    But i change D2 and D3, then the value of A cycles  remains constant 256ppr, it doesn't change

Children
No Data