Product Number: I want to generate sine wave using the AD5941?
Software Version: STM32 MCU + https://github.com/analogdevicesinc/ad5940-examples/tree/master/examples/AD5940_WG example code
Hi folks,
I want to generate sine wave using AD5941, and need to project that on digital analyzer.
I am running following code to generate the sine wave:
void AD5940_Wg_Test(void) { AFERefCfg_Type aferef_cfg; HSLoopCfg_Type HsloopCfg; CLKCfg_Type clk_cfg; clk_cfg.ADCClkDiv = ADCCLKDIV_1; clk_cfg.ADCCLkSrc = ADCCLKSRC_HFOSC; clk_cfg.SysClkDiv = SYSCLKDIV_1; clk_cfg.SysClkSrc = SYSCLKSRC_HFOSC; clk_cfg.HfOSC32MHzMode = bFALSE; clk_cfg.HFOSCEn = bTRUE; clk_cfg.HFXTALEn = bFALSE; clk_cfg.LFOSCEn = bTRUE; AD5940_CLKCfg(&clk_cfg); aferef_cfg.HpBandgapEn = bTRUE; aferef_cfg.Hp1V1BuffEn = bTRUE; aferef_cfg.Hp1V8BuffEn = bTRUE; aferef_cfg.Disc1V1Cap = bFALSE; aferef_cfg.Disc1V8Cap = bFALSE; aferef_cfg.Hp1V8ThemBuff = bFALSE; aferef_cfg.Hp1V8Ilimit = bFALSE; aferef_cfg.Lp1V1BuffEn = bFALSE; aferef_cfg.Lp1V8BuffEn = bFALSE; /* LP reference control */ aferef_cfg.LpBandgapEn = bTRUE; aferef_cfg.LpRefBufEn = bTRUE; aferef_cfg.LpRefBoostEn = bFALSE; AD5940_REFCfgS(&aferef_cfg); HsloopCfg.HsDacCfg.ExcitBufGain = EXCITBUFGAIN_2; HsloopCfg.HsDacCfg.HsDacGain = HSDACGAIN_1; HsloopCfg.HsDacCfg.HsDacUpdateRate = 7; HsloopCfg.HsTiaCfg.DiodeClose = bFALSE; HsloopCfg.HsTiaCfg.HstiaBias = HSTIABIAS_1P1; HsloopCfg.HsTiaCfg.HstiaCtia = 16; /* 16pF */ HsloopCfg.HsTiaCfg.HstiaDeRload = HSTIADERLOAD_OPEN; HsloopCfg.HsTiaCfg.HstiaDeRtia = HSTIADERTIA_TODE; HsloopCfg.HsTiaCfg.HstiaRtiaSel = HSTIARTIA_160K; HsloopCfg.SWMatCfg.Dswitch = SWD_CE0; HsloopCfg.SWMatCfg.Pswitch = SWP_CE0; HsloopCfg.SWMatCfg.Nswitch = SWN_SE0LOAD; HsloopCfg.SWMatCfg.Tswitch = SWT_TRTIA|SWT_SE0LOAD; HsloopCfg.WgCfg.WgType = WGTYPE_TRAPZ; HsloopCfg.WgCfg.GainCalEn = bFALSE; HsloopCfg.WgCfg.OffsetCalEn = bFALSE; HsloopCfg.WgCfg.TrapzCfg.WGTrapzDCLevel1 = 0x200; HsloopCfg.WgCfg.TrapzCfg.WGTrapzDCLevel2 = 0xa00; HsloopCfg.WgCfg.TrapzCfg.WGTrapzDelay1 = 50; HsloopCfg.WgCfg.TrapzCfg.WGTrapzDelay2 = 100; HsloopCfg.WgCfg.TrapzCfg.WGTrapzSlope1 = 200; HsloopCfg.WgCfg.TrapzCfg.WGTrapzSlope2 = 300; AD5940_HSLoopCfgS(&HsloopCfg); AD5940_AFECtrlS(AFECTRL_DACREFPWR, bTRUE); AD5940_AFECtrlS(AFECTRL_EXTBUFPWR|AFECTRL_INAMPPWR|AFECTRL_HSTIAPWR|AFECTRL_HSDACPWR, bTRUE); AD5940_AFECtrlS(AFECTRL_WG, bTRUE); AD5940_AFEPwrBW(AFEPWR_LP, AFEBW_250KHZ); }
which pin is the target pin to see the sinewave using this code? I am not able to get sine wave using this code, when I am trying to get output from CE0 pin ?
Any suggestion or rectification would be helpful.
which pin to project on digital analyzer, whether the code I am running is correct or not?