Hi, I'm using EVAL-AD4110-1SDZ evaluation board and the SDP-K1 board to run the EVAL-AD4110 firmware.
The AD4110 chip is always in error with the corresponding red led on.
I've modified the code in order to debug. Leaving only the software reset SPI communication (a sequence of 8 0xFF from the interface controller to the AD4110-1 chip) the result is the same.
The low level SPI communication seams to be correct using a logic state analyzed.
Theorically the firmware was developed expressly for this two boards so it should have been a plug and play test.
Thanks
Carlo L.