Post Go back to editing

AD7903 - can it do +/-5v differential input?

Category: Datasheet/Specs
Product Number: AD7903

Dear ADI,

I have two a low-impedance source of two (2) differential analog channels/voltages (X and Y) that are both +/-5v (ie: +/-10v SE equivalent) and I would like to sample them with the AD7903 - am I able to just wire those signals directly into the AD7903 as follows without the need of any drivers ? :-

+X (-5v..+5v) -> IN1+

-X (-5v..+5v) -> IN1-

+Y (-5v..+5v) -> IN2+

-Y (-5v..+5v) -> IN2-

Thanks very much!

Cheers,

Rodney