Post Go back to editing

About AD2S83 component-selection.exe which the software cannot run under the main Windows operating system of personal computer At present

Category: Hardware
Product Number: AD2S83
Software Version: N/A

About AD2S83 component-selection.exe which the software cannot run under the main Windows operating system of personal computer At present, 

1. Are there any new available software tools to replace it ?

2.Working frequency: 400Hz, selection accuracy: 16 bits, who can give the values of R1, C1, R2, C2, R3, C3, R4, C4, R5, C5, R6, C6, R7, C7 ?

Parents Reply
  • 1. DOSBox setup

    link:pan.baidu.com/.../1UwSpoh9mU0PtJ00BF63zRA

    code:hiaj

    2.run DOSBox0.74-win32-installer * exe files setup ,click Next is ok

    3.open DOSBox

    Firstly, use a command to treat our file directory as a virtual C drive, and the sentence in the image will display, meaning that the virtual operation has been successfully completed.

    mount c d:\dosbox\ad2s83

           => mount:The meaning of preparation and arrangement;

           => c:Indicates to be virtual as a C drive;

           => d:\dosbox\ad2s83: 

Children
No Data