Post Go back to editing

About AD2S83 component-selection.exe which the software cannot run under the main Windows operating system of personal computer At present

Category: Hardware
Product Number: AD2S83
Software Version: N/A

About AD2S83 component-selection.exe which the software cannot run under the main Windows operating system of personal computer At present, 

1. Are there any new available software tools to replace it ?

2.Working frequency: 400Hz, selection accuracy: 16 bits, who can give the values of R1, C1, R2, C2, R3, C3, R4, C4, R5, C5, R6, C6, R7, C7 ?

Parents Reply
  • Thanks for sharing. I made it run on DOSBOX as well. Are you designing AD2S83 application? Just curious to ask why you selected the AD2S83? May we know your application that it fits the AD2S83, if that is OK to share. And do you find the tool helpful and what else needs to improve on this tool.

    Regards,

    Jonathan

Children
  • 1. DOSBox setup

    link:pan.baidu.com/.../1UwSpoh9mU0PtJ00BF63zRA

    code:hiaj

    2.run DOSBox0.74-win32-installer * exe files setup ,click Next is ok

    3.open DOSBox

    Firstly, use a command to treat our file directory as a virtual C drive, and the sentence in the image will display, meaning that the virtual operation has been successfully completed.

    mount c d:\dosbox\ad2s83

           => mount:The meaning of preparation and arrangement;

           => c:Indicates to be virtual as a C drive;

           => d:\dosbox\ad2s83: