Post Go back to editing

AD7903 Datasheet Specs

Category: Hardware
Product Number: AD7903

Hello,

I have been looking through ADCs to find one which can sample sinusoidal signal whose frequency varies between 100Hz and 20kHz. AD7903 is a good option for me so far. However, I have some concerns. In the datasheet here https://www.analog.com/media/en/technical-documentation/data-sheets/AD7903.pdf in figure17 and figure20 no data is displayed for frequencies lower than 20kHz. I assume SINAD and THD improve at lower frequencies. But I still have concerns. Do you think I can sample 100Hz sinusoidal signals without introducing any degradation to the signal? Are there any other ADCs that you can suggest?

Best regards.