Hi,
We using LTC2496 ADC which is connected to our micro control using SPI. we are trying to read the conversion value through channel 11 (configured as single ended and the reference voltage is set to 5V) by giving a voltage of 2.5 V for testing purpose .But when we are reading the channel, we are receiving zero as data , we have verified all the wave forms and connections ,everything is according to the data sheet.
Below is the DATA FORMAT (MSB First) and link for data sheet we are referring to :
Byte #1 Byte #2 Byte #3
1 0 EN SGL OS S2 S1 S0 X X X X X X X X X X X X X X X X
Data In : 1 0 1 1 1 1 0 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
!EOC DMY SIG MSB D15 D14 D13 D12 D11 D10 D9 D8 D7 D6 D5 D4 D3 D2 D1 D0 - - - -
Data Out : 0 0 1 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 - - - -
Data sheet : https://www.analog.com/media/en/technical-documentation/data-sheets/2496fc.pdf
Can you please let us know what is causing this issue
Regards,
Revathi