Hi,
I have been using the AD573, but since it is a newly developed deprecated product, So I have been looking for an alternative, and the AD1674TDseems to work.
(I chose the AD1674TD because it must support a temperature range of -55°C and ±5 V input.)
However, the AD1674 datasheet does not include a reference circuit. There is no evaluation board either.
Are there any reference circuits or documents that can be used as a reference for the design?
I posted the same thing in the Reference Designs column first, but I was advised to post it in the Precision AD Converter column.
Regards,
Kazu