Hi,
I am working on AD6676 chip,I have a doubt on PIN_0DBFS calculation, as per the equations(2) & (4) given in pg no - 28 and 29 in the datasheet of AD6676,will my PIN_0DBFS value change just by writing to the register 0x10A.
Also as per calculations based on both the equations I have got PIN_0dBFS = 10 × log10(1/2 × RIN × IDAC1FS2) as -33.1876 and if I change the IDAC1_FS value from 0x40 to 0x20 (PIN_0dBFS = -39.208) in the equation ,then I can see a 6dB difference between both as mentioned in pg no - 71 for register 0x10A (IDAC1FS Gain Scaling Register) .
But when I change the value from 0x40 to 0x20 in the register 0x10A, I am not able to observe any changes in fundamental amplitude in the output samples when plotted.
I need to configure PIN_0dBFS to -2.7dBm as mentioned in one of the example in the datasheet ,so can u please provide with the configuration changes that needs to be done.