Post Go back to editing

AD5941 Impedance example Vzero setting

Category: Software
Product Number: AD5941
Software Version: master

Hey,

In the Impedance example whenever a DC voltage is applied, the VZero is also set to half of it's maximum range. I can see this been done 

line 260 of impedance.c is

    lpdac_cfg.DacData6Bit = 0x40>>1;            /* Set Vzero to middle scale. */

but why is it set to the middle of the scale? Does that not just lower the maximum possible bias applied since the bias is the difference between Vzero and VBias?