Post Go back to editing

AD4134 DIG_FILTER_OFUF overflow

Thread Summary

The user is experiencing channel overflow and filter set errors with the AD4134 when using a 4-channel sinc3 filter. The issue with registers 40, 41, and 42 changing values was resolved by setting High Performance Mode. However, the DCLK error persists due to a mismatch between the specified 48MHz DCLK and the 12MHz setting in register 0x11 (0x20). The user should verify the DCLK configuration and ensure correct input to AVDD1V8, DVDD1V8, and CLKVDD.
AI Generated Content
Category: Software

Hello,

I'm looking at the AD4134,but when I set 4-channel-sinc3 filter,always has channel say overflow and  channel filter set error ,this is my reading register :

System V0.0.42 Jan 5 2023 10:16:46
spi0_init self test succ
spi test start!

AD4134 reg00 = 0x18
AD4134 reg01 = 0x80
AD4134 reg02 = 0xE0
AD4134 reg03 = 0x07
AD4134 reg04 = 0x39
AD4134 reg05 = 0x5C
AD4134 reg06 = 0x00
AD4134 reg07 = 0x02
AD4134 reg08 = 0x00
AD4134 reg09 = 0x00
AD4134 reg0A = 0x00
AD4134 reg0B = 0x02
AD4134 reg0C = 0x56
AD4134 reg0D = 0x04
AD4134 reg0E = 0x00
AD4134 reg0F = 0x00
AD4134 reg10 = 0x00
AD4134 reg11 = 0x20
AD4134 reg12 = 0x02
AD4134 reg13 = 0x02
AD4134 reg14 = 0x00
AD4134 reg15 = 0x21
AD4134 reg16 = 0x40
AD4134 reg17 = 0x00
AD4134 reg18 = 0x00
AD4134 reg19 = 0x72
AD4134 reg1A = 0xB7
AD4134 reg1B = 0xCE
AD4134 reg1C = 0x2B
AD4134 reg1D = 0x00
AD4134 reg1E = 0xAA
AD4134 reg1F = 0x00
AD4134 reg20 = 0x00
AD4134 reg21 = 0xEF
AD4134 reg22 = 0x00
AD4134 reg23 = 0x00
AD4134 reg24 = 0x00
AD4134 reg25 = 0x00
AD4134 reg26 = 0x00
AD4134 reg27 = 0x00
AD4134 reg28 = 0x00
AD4134 reg29 = 0x00
AD4134 reg2A = 0x00
AD4134 reg2B = 0x00
AD4134 reg2C = 0x00
AD4134 reg2D = 0x00
AD4134 reg2E = 0x00
AD4134 reg2F = 0x00
AD4134 reg30 = 0x00
AD4134 reg31 = 0x00
AD4134 reg32 = 0x00
AD4134 reg33 = 0x00
AD4134 reg34 = 0x00
AD4134 reg35 = 0x00
AD4134 reg36 = 0x00
AD4134 reg37 = 0x00
AD4134 reg38 = 0x00
AD4134 reg39 = 0x00
AD4134 reg3A = 0x00
AD4134 reg3B = 0x00
AD4134 reg3C = 0x00
AD4134 reg3D = 0x00
AD4134 reg3E = 0x00
AD4134 reg3F = 0x00
AD4134 reg40 = 0x0F
AD4134 reg41 = 0x0C
AD4134 reg42 = 0x08
AD4134 reg43 = 0x00
AD4134 reg44 = 0x00
AD4134 reg45 = 0x00
AD4134 reg46 = 0x00
AD4134 reg47 = 0x00
AD4134 reg48 = 0x00

every time I download code, the reg40/41/42 will change,How can I fix this?

Parents Reply Children
  • Hi  ,

    Please see comments below. Thank you.

    • Digital filter overflow
      • Can you try to read back the registers upon power up before applying input?
    • Filter not settled
      • What channels are you using? What values are you reading from the register 0x41? From the previous data, digital filter for Channels 0 and 1 are settled.
    • DCLK ERROR
      • You have mentioned you are using DCLK 48MHz but register 0x11 is set to 0x20 where the DCLK is 12MHz. This may be the reason for the DCLK error.
    • Kindly provide the schematic and register values upon power up.
    • Are you providing correct input to AVDD1V8, DVDD1V8, and CLKVDD?

    Thanks,

    Janine

  • Only one question remains, register 0x11 set to 0x20 means Bits:0010-0000,  ,I got it from datasheet 24-bit ADC data only and DCLK=48MHz, I don't understand why the DCLK is 12MHz?     0010 is Bits-7:4 0000 is Bits 3:0 ? How can I set the DCLK 48MHz by register 0x11? 

  • Hi  ,

    You are correct. The DCLK is set to 48MHz. I apologize for the confusion. Are you still encountering the DCLK error?