I want to put a resistor in the front stage and adjust the gain.
What is the input impedance of the ADuM7702?
add FIG
[edited by: UBOTI at 7:33 AM (GMT -5) on 20 Dec 2022]
ADUM7702
Recommended for New Designs
The ADuM7702 is a high performance, second-order, S-? modulator that converts an analog input signal to a high speed, single-bit data stream, with on-chip...
Datasheet
ADUM7702 on Analog.com
I want to put a resistor in the front stage and adjust the gain.
What is the input impedance of the ADuM7702?
Hi,
In the analog input section of the datasheet it is written: "The pseudo differential analog input of the ADuM7702 is implemented with a switched capacitor circuit.". So it means dynamic load rather than resistive, what is specified:
In the examples 10 Ohm external impadance can be seen, so I think it is not recommended to use higher, because due to the dynamic input current it will introduce error. Taking the 10 Ohm at full-scale input you just get an error close to the resolution of the ADC.
Zoltan
Thank you for your answer