The data sheet for AD7770 describes daisy chaining but does not explain how the SPI data is recovered. Does each device have its own SPI connection or is it only the last ADC in the chain?
AD7770
Recommended for New Designs
The AD7770 is an 8-channel, simultaneous sampling ADC. Eight
full sigma-delta (Σ-Δ) ADCs are on chip. The AD7770 provides
a low input current to allow...
Datasheet
AD7770 on Analog.com
The data sheet for AD7770 describes daisy chaining but does not explain how the SPI data is recovered. Does each device have its own SPI connection or is it only the last ADC in the chain?
Hi davec ,
Only the last ADC in the chain has SPI connection to the digital host. In daisy chain mode, the data is propagated from one subnode to the next. Please have a look at the links below for more details on daisy-chain. Thank you!
https://www.analog.com/en/analog-dialogue/articles/introduction-to-spi-interface.html
https://www.analog.com/media/en/technical-documentation/tech-articles/daisychaining-spi-devices.pdf
Thanks,
Janine
Janine,
Thanks for that. For a configuration with two 8 channel ADCs the SPI data stream would have alternate 16 bit data samples from each ADC. The first ADC would have all the odd numbered channels and the other ADC the even ones.
Janine,
Happy New Year.
Unfortunately we are still unable to find definitive details on daisy chaining the AD7770 ADC in SDI mode. In the technical manual for the AD76630 ADC the wiring and data format is well described. Please advise where we can find the equivalent information for the AD7770.
Regards,
Dave Courtney
Hi davec ,
Daisy chain mode is only available in DOUT interface and not in SPI interface.
When using daisy chain, DOUT2 and DOUT3 act as input pins that will receive yes data from the previous ADC.
DOUT is not a standard SPI and the ADC generates the clock in daisy chain mode.
Please refer to the figure below for the daisy chain mode configuration using 2 DOUT lines.
Thanks,
Janine
Hi davec ,
I'm glad we could help. We have added 2 new FAQs for AD777x that may further explain this in case others also encounter the same queries.
AD777x: How to configure AD777x in daisy chain mode?
AD777x: How to synchronize multiple AD777x?
Thanks,
Janine
Hi davec ,
I'm glad we could help. We have added 2 new FAQs for AD777x that may further explain this in case others also encounter the same queries.
AD777x: How to configure AD777x in daisy chain mode?
AD777x: How to synchronize multiple AD777x?
Thanks,
Janine