Post Go back to editing

AD7147 for Water Level Sensing

Product Number: AD7147ACPZ-1500RL7

Hi,

We have been working on a water level sensing application with the AD7147ACPZ-1500RL7 chip, we use two aluminum plates as a sensor, one is connected to the CIN0 pin, and the other one is connected to the ground. Stage0 is used for CIN0 CDC conversion.

The sensor is fixed inside the plastic container, and we increased the water level for 0.5cm each time and monitored the Bank-1 register "0X00B" value periodically.

following are the configuration used in our application

Bank-1 register:


0x00 = 0x0210
0x01 = 0x0000
0x02 = 0x000B
0x03 = 0x0000
0x04 = 0x0000
0x05 = 0x0000
0x06 = 0x0000
0x07 = 0x0000

Bank-2 register: (For Stage0)


0x80 = 0xFFFE
0x81 = 0x1FFF
0x82 = 0x0000
0x83 = 0x0000
0x84 = 0
0x85 = 0
0x86 = 0
0x87 = 0

For our test case, we don't need any interrupts and thresholds, so we left those register values as zero.


Test case observation:

The CDC result doesn't change gradually with respect to the water level,

For example,

The CDC result is in its mid-value (32767) at the beginning, once we start pouring water into the container we expect the CDC to change gradually but the CDC doesn't change for water levels from 0 - 2cm, but when we pour an extra 0.5cm of water the CDC drastically changes from its mid-value 32767 to 46420. And the CDC result stayed at this value for water levels 2.5 - 4.5cm. When we add an extra 0.5cm of water the CDC reaches its max value of 65535.

Expected result:

CDC result should change for every 0.5cm of water level.

Circuit Design:

The voltage of VCC and VDRIVE is 3.3v

Q:

1. Is this the correct way to sense the water level?
2. Should we need any other register configuration?


Thank You,

Siva

  • Hi Siva, The AD7174 is not designed for this application and there are more suitable devices for water level sensing as described in this article
    https://www.analog.com/en/analog-dialogue/articles/liquid-level-sensing-using-cdcs.html

    The AD7147 is a self capacitance (grounded sensor) measurement device. Mutual capacitance (floating sensor) measurement is more effective for water level measurement as described in the article. The AD7142 is a mutual capacitance measurement equivalent of the AD7147.

    Having said that it should work but it is critically dependent on the design of the sensor electrodes, can you provide details of the sensor construction, e.g. the sizes of the aluminum plates, the distance between them, how they are positioned relative to each other, how the water interacts with the plates.

    As a quick check, If you gradually bring your finger closer to the CIN0 plate do you see an increasing result ?

    Regards,

    Maurice.

  • Hi Maurice,

    Thank you for your information.

    I share our sensor details below,

    Material: Aluminum Plate
    Shape: Rectangle
    Width: 2mm
    Height: 4cm
    Distance b/w them: 1cm

    Q: how they are positioned relative to each other
    A: The two plates are placed beside each other.

    Q: how the water interacts with the plates?
    A: The sensor is placed inside a plastic container covered with a thin plastic cover. The water we pour inside the container will have contact with that plastic cover.

    The left side plate is connected to the ground and the right side plate is connected to the CIN0.


    Q: If you gradually bring your finger closer to the CIN0 plate do you see an increasing result?
    A: When the sensor is placed inside the container, the result doesn't change until my finger partially touches the sensor. Once my finger touches the sensor the result increases non-linearly.

  • Hi Siva, If the plates were made wider and placed closer together you should get improved sensitivity and a more linear response. with the sensor as it is I think that the response is too small and only responds to large changes in water level.

  • Hi Maurice,

    We have already tried the wider and closer plates,

    Material: Aluminum Plate
    Shape: Rectangle
    Width: 1cm
    Height: 9cm
    Distance b/w them: 5mm

    But the CDC reaches its max value for smaller changes in water level (1.5cm or 2cm of water level) also the change seems to be as same as the sensor mentioned above, but the difference is the change occurred in more minor water level changes. That's why we moved to this sensor.

    with the sensor as it is I think that the response is too small and only responds to large changes in water level.

    Q: Even though the response is too small and only responds to a large change in water level, why it has to be this level of increase in the result (i.e. more than a 10k difference), does it is the expected response?

    We also tried different sensors with different sizes. All the sensor's results stayed near the mid-value (32,767) for some water levels and then jumped to 46,420. The only difference is, the change in CDC results occurs at different water levels.

    Q: why it has to be a similar type of CDC response for different sensor plates?

  • Hi Siva, If you shift the initial value away from mid point, to 50k for example do you see the same situation ?

  • Hi Maurice,

    Sorry for the late reply.

    We ain't test that.
    Right now we were working on some other projects, so will test that later and let you know the result.

    Thank you.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.