Post Go back to editing

AD74413RBCPZ Reference voltage change

Category: Hardware
Product Number: AD74413RBCPZ

Hi,

I have three AD74413RBCPZ on a PCB. All three are configured as 4-20mA output DACs

For two of the parts, Refout is 4.99V and 4.98V. For the third one, it is 2.63V. 

For the third part, the current output is beyond the specified tolerance.

Since the Refout is generated internally, there is nothing which can be checked other than measuring the Refout V.

The Refout is shorted with Refin with a 100nF decoupling capacitor.

What could be wrong? How can the Reference be corrected?

This problem is local to one PCB, others are working fine.

Thanks,

JPD



spelling mistake corrected
[edited by: JPD at 3:06 PM (GMT -5) on 12 Dec 2022]
Parents
  • Hi JPD,

    if the problem appears only at one AD74413R part, I would suggest to replace the part for the new one. 

    Output voltage of the Reference cannot be adjusted. I believe, that internal Reference of the part might be damaged.

    Regards,

    Arnost

  • Hi Arnost,

    What could be the reason for the damage? How can we prevent it from happening again?

    Regards,

    JPD

  • Hi JPD,

    nature of the issue is still unknown to me.

    Does replacing one part helped you to solve the issue? This would indicate that something was damaged at that particular piece of AD74413R.

    I would indicate that stressing part above Absolute maximum rating specified in datasheet might cause the problem.  (In this case REFIN or REFOU T -0.3V to +5V.)

    Increase voltage at REFOUT pin might indicate, that pin is loaded by current. Could you please check the capacitor, if it is not shorted or damaged. 

    If still have part at your board, I would also check all voltages as AVDD, ALDO5V, DVCC, ALDO1V8 and AVSS. This might provide more insights to us.

    If you can communicate with it, could you provide "ALERT_STATUS" register reading. 

    Regards,

    Arnost

  • Hi Arnost,

    Thank you for the inputs.

    Well, my Testing team informs me that  AVDD, ALDO5V, DVCC, ALDO1V8 and AVSS. are all within specs, and replacing all MLCCs around the part have made absolutely no difference.

    Replacing the defective part made the board functional.

    We are at a total loss when it comes to finding the root cause.. causing serious doubts about the robustness of the AD74412R. The part is a wee bit expensive, and we are not happy reworking PCBs for no apparent reasons.

    Regards,

    JPD

Reply
  • Hi Arnost,

    Thank you for the inputs.

    Well, my Testing team informs me that  AVDD, ALDO5V, DVCC, ALDO1V8 and AVSS. are all within specs, and replacing all MLCCs around the part have made absolutely no difference.

    Replacing the defective part made the board functional.

    We are at a total loss when it comes to finding the root cause.. causing serious doubts about the robustness of the AD74412R. The part is a wee bit expensive, and we are not happy reworking PCBs for no apparent reasons.

    Regards,

    JPD

Children