Post Go back to editing

ADC wrong values AD74412R

Category: Hardware
Product Number: AD74412R

Hello,
I have designed a board with the AD74412R and the thing is that I am having problems getting it to work to measure voltage (ADC).

The configuration of registers that I get once the board starts reading through the SPI I think is correct.

If I apply a voltage of 5.00V to the four inputs and configure through the SPI for ADC mode (range 0-10v), the status of the registers is as follows:

(column with values "after reset" and column "configured" after configuracion)

Address (DEC) Address (HEX) Name value after reset value configured comment
0 0 NOP 0x0 0x0  
1 1 CH_FUNC_SETUPA 0x0 0x3 voltage input, which measures the voltage across the I/OP_x to I/ON_x screw terminals.
2 2 CH_FUNC_SETUPB 0x0 0x3 voltage input, which measures the voltage across the I/OP_x to I/ON_x screw terminals.
3 3 CH_FUNC_SETUPC 0x0 0x3 voltage input, which measures the voltage across the I/OP_x to I/ON_x screw terminals.
4 4 CH_FUNC_SETUPD 0x0 0x3 voltage input, which measures the voltage across the I/OP_x to I/ON_x screw terminals.
5 5 ADC_CONFIGA 0x0 0x4 voltage between the I/OP_x screw terminals and the AGND_SENSE pin. Enable 200Kohm. Disable 50hz reject
6 6 ADC_CONFIGB 0x0 0x4 voltage between the I/OP_x screw terminals and the AGND_SENSE pin. Enable 200Kohm. Disable 50hz reject
7 7 ADC_CONFIGC 0x0 0x4 voltage between the I/OP_x screw terminals and the AGND_SENSE pin. Enable 200Kohm. Disable 50hz reject
8 8 ADC_CONFIGD 0x0 0x4 voltage between the I/OP_x screw terminals and the AGND_SENSE pin. Enable 200Kohm. Disable 50hz reject
9 9 DIN_CONFIGA 0xb 0xb  
10 A DIN_CONFIGB 0xb 0xb  
11 B DIN_CONFIGC 0xb 0xb  
12 C DIN_CONFIGD 0xb 0xb  
13 D GPO_PARALLEL 0x0 0x0  
14 E GPO_CONFIGA 0x0 0x0  
15 F GPO_CONFIGB 0x0 0x0  
16 10 GPO_CONFIGC 0x0 0x0  
17 11 GPO_CONFIGD 0x0 0x0  
18 12 OUTPUT_CONFIGA 0x0 0x0  
19 13 OUTPUT_CONFIGB 0x0 0x0  
20 14 OUTPUT_CONFIGC 0x0 0x0  
21 15 OUTPUT_CONFIGD 0x0 0x0  
22 16 DAC_CODEA 0x0 0x0  
23 17 DAC_CODEB 0x0 0x0  
24 18 DAC_CODEC 0x0 0x0  
25 19 DAC_CODED 0x0 0x0  
26 1A DAC_CLR_CODEA 0x0 0x0  
27 1B DAC_CLR_CODEB 0x0 0x0  
28 1C DAC_CLR_CODEC 0x0 0x0  
29 1D DAC_CLR_CODED 0x0 0x0  
30 1E DAC_ACTIVEA 0x0 0x0  
31 1F DAC_ACTIVEB 0x0 0x0  
32 20 DAC_ACTIVEC 0x0 0x0  
33 21 DAC_ACTIVED 0x0 0x0  
34 22 DIN_THRESH 0x0 0x0  
35 23 ADC_CONV_CTRL 0x0 0x50f Enables conversions on Channel A,B,C,D. Starts single sequence conversion
36 24 DIAG_ASSIGN 0x0 0x0  
37 25 DIN_COMP_OUT 0x0 0x0  
38 26 ADC_RESULTA 0x0 0x641d (25629/65535)*10 = 3.91 volts
39 27 ADC_RESULTB 0x0 0x635b (25435/65535)*10 = 3.88 volts
40 28 ADC_RESULTC 0x0 0x6382 ..
41 29 ADC_RESULTD 0x0 0x6304 ..
42 2A DIAG_RESULTA 0x0 0x0  
43 2B DIAG_RESULTB 0x0 0x0  
44 2C DIAG_RESULTC 0x0 0x0  
45 2D DIAG_RESULTD 0x0 0x0  
46 2E ALERT_STATUS 0x0 0x0  
47 2F LIVE_STATUS 0x0 0x4000 ADC_DATA_RDY
48 30 ALERT_MASK 0x0 0x0  
49 31   0x0 0x0  
50 32   0x0 0x0  
51 33   0x0 0x0  
52 34   0x0 0x0  
53 35   0x0 0x0  
54 36   0x0 0x0  
55 37   0x0 0x0  
56 38   0x0 0x0  
57 39   0x0 0x0  
58 3A   0x0 0x0  
59 3B   0x0 0x0  
60 3C ALERT_MASK 0x0 0x0  
61 3D   0x0 0x0  
62 3E   0x0 0x0  
63 3F   0x0 0x0  
64 40   0x0 0x0  
65 41 READ_SELECT 0x41 0x41  
66 42 ADC_CONV_CTRL_80SPS 0x0 0x0  
67 43 THERM_RST 0x0 0x0  
68 44 CMD_KEY 0x0 0x0  
69 45 SCRATCH 0x0 0x0  
70 46 SILICON_REV 0x8 0x8  


As you can see, the value of the registers related to the ADCs show values of 3.91V and not 5.00V as expected.

What could be wrong?
I have checked the voltages and everything seems to be within the correct range.
I have tried a multitude of tests, both firmware and HW, but I never get the correct values.

Say that if I configure the DAC voltage output from 0 to 10V it works correctly

Regarding the board itself, say that the analog part is identical to the evaluation board. I've been through it dozens of times

I would be very grateful if you could help me.

thank you in advance

  • Say that if I configure the DAC voltage output from 0 to 10V it works correctly

    Well, to be right, de rang I get is from 0 to 11 volts  instead expected 10v.   could it be related with problems with ADC I'm getting?

  • Hi,

    We will look into this. I will contact the product owner and get back to you.

    Regards,

    JC

  • Hi,

    I am product application engineer on this part, I would be happy to support you. 

    Thank you for providing full read of the register map, that was very helpful for check, to me part seems to be configured correctly.

    Let me ask couple more clarifying questions:

    # Could you please check and provide all on board voltages (AVDD, DVCC, DLDO1V8, IOVDD, ALDO1V8, AVSS, ALDO5V)

    # What is the source of your channel input voltage in this experiment? 

    # Are you using internal or external reference? 

    # Let me double check, if following delay is not issue at your setup: "The user must wait 100 μs before starting
    conversions." (ADC_CONV_CTRL: CONV_SEQ: 01: starts single sequence ... powers up the ADC. The user must wait 100 μs before starting
    conversions.)

    Regards,

    Arnost

  • Hello Arnost,
    I really appreciate your answer to the problem I have.


    # I have checked the values of the voltages again:

    AVDD: 14.35V
    DVCC: 3,289V
    DLDO1V8: 1,799V
    IOVDD: 3,289V
    ALDO1V8: 1,795V
    AVSS: -2,583V !!! Shouldn't it be -3.3V? Could the problem be here?
    REFIN = REFOUT = 2.494V (connected together)
    ALDO5V = 4.996V

    # The power supply for the analog inputs is a RIGOL DP832. Also tested with a 1.5V battery (to avoid 50/60Hz problems...).

    # I am using internal reference. REFIN = REFOUT = 2.494V

    # I have already added 100mS delays between commands or SPI accesses to prevent this problem.

    What do you think could be the problem?

    Thank you in advance,

    Best regards,

  • Hi,

    Low AVSS might indicate damaged charge pump, it should generate -DVCC.

    I would suggest to look, if AVSS does not drop during ADC measurements. (Probably turn on ADC to continuous measurement and measure AVSS.) 

    Regards,

    Arnost

  • I have monitored the AVSS voltage and have seen the following:

    Apparently I see that there are small oscillations of the AVSS value just when I configure the ADC in single conversion. The voltage variation is around 50mV. I understand that this should not be the problem.
    What do you think? Any other cause for this AVSS different than expected -DVCC?

    Maybe the IC is damaged internally?

    thank you for your support,

    Regards,

  • Hi,

    I am little concerned about absolute value of the AVSS. At two boards I have measured, I also have 3V3 DVCC and generated AVSS value around -3.2V

    It is worthy of try another part.

    Please keep me posted, one you will have update. 

    Regards,

    Arnost

  • Hi Arnost,

    Well, finnally I've changed the IC and now seems to work fine.

    Thank you!

    Best regards,

  • Hi  ,

    thank you very much for your feedback.

    I am happy, you are setup running. 

    Regards,

    Arnost