AD4134
Recommended for New Designs
The AD4134 is a quad channel, low noise, simultaneous sampling, precision analog-to-digital converter (ADC) that delivers on functionality, performance...
Datasheet
AD4134 on Analog.com
Hi,
I am looking for some clarification regarding synchronisation of 8 AD4134 devices with common MCLK and common ODR signals.
I note in the datasheet that a DIG_IF_RESET is required to ensure device-to-device synchronisation. It is not clear what ODR or DCLK should be doing when we apply this reset. Or indeed whether there needs to be a defined relationship between ODR and the SPI broadcast to all devices.
We are seeing very mixed results operating the ADC at 1 MSPS. A large proportion of captures seem to be out of phase by an entire ODR clock period, that is some chips are in one phase while the rest are in another (see attached plots sampling rising edge of square wave).
A DIG_IF_RESET is applied between the shots in the attached PDF. This reset is applied by a hardware process, after the falling edge of ODR, and consists of an SPI write to reg 0x01 with data equal to 0x82. The ADC is constantly sampling throughout, (constant ODR and gated DCLK).
Any further guidance you can provide would be much appreciated.
Regards,
S Robson
Hi srobson ,
Can you help provide additional details on your setup and the schematic layout for the 8 ADCs?
Please note that the connection from the controller to the 8 AD4134 devices should be identical since a small layout mismatch could result in a phase mismatch.
Thanks,
Janine
Hi Janine,
Is there anything further you can contribute on this?
Thanks,
Scott
Hi Scott,
Apologies for getting back to you just now. Can you include DCLK in the signal trace? Please note DIG_IF_RESET should be issued simultaneously to all devices after ODR and DCLK.
Thanks,
Janine
Hi Scott,
Apologies for getting back to you just now. Can you include DCLK in the signal trace? Please note DIG_IF_RESET should be issued simultaneously to all devices after ODR and DCLK.
Thanks,
Janine