I would like to ask about the ADC drive AMP built into the ADAQ7980.
I'm considering using it in an inverted AMP configuration. How far from the power rail do the outputs go?
(What is the headroom voltage?)
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
ADAQ7980
Recommended for New Designs
The ADAQ7980/ADAQ7988 are 16-bit analog-to-digital converter
(ADC) μModule® data acquisition systems that integrate four common signal processing and...
Datasheet
ADAQ7980 on Analog.com
I would like to ask about the ADC drive AMP built into the ADAQ7980.
I'm considering using it in an inverted AMP configuration. How far from the power rail do the outputs go?
(What is the headroom voltage?)
Hi UBOTI ,
We will look into this. I will contact the product owner and get back to you.
Regards,
JC
Thank you.
I am concerned about how well the linearity is maintained.
Hi UBOTI ,
Regarding the output headroom voltage, we will contact the designer of this micromodule. May I ask what specific application or other details that you can share (i.e., gain, power rails, etc.)?
Regarding the linearity, you may refer to these specs and TPC from the datasheet:


Please note that these specifications are in unity-gain configuration.
I am inquiring about the linearity of the drive AMP.
The condition of the answer you gave me is meaningless because the input of the drive AMP is not equal to the power supply V+ of the drive amp.
When used with V+=5V, REFOUT=5V, with IN=5V input (inverted AMP configuration)
(not use internal BUFFAMP)

I inquired about how much input accuracy is
Who is the μ module designer contact person?
Hi Chelsea ,
Could you please confirm the output swing of ADC input driver?
The end customer is asking what is the output headroom of the driver AMP.
Hi UBOTI ,
Thank you again for reaching out to us and I apologize for the confusion, I understood it as the linearity in ADCs.
The output swing of the ADAQ7980’s ADC driver would require at least 20mV headroom/footroom — which was characterized with a relatively light resistive load (not an ADC).
Please note that for your use case of V+ = REF_OUT = 5V, in an inverting configuration, you will have to accept the slight loss in the output range (i.e., cannot use the full input range of the ADC). To have a linear output from 0V to VREF, it is suggested to:
It was very helpful.
Thank you.