Post Go back to editing

What is the recommended Microcontroller for reading from AD7381-4 Quad-SPI like interface

Category: Hardware
Product Number: AD7381-4

The AD7381-4 uses an enhanced SPI digital interface with CS, SCLK, SDI, and 4 SDO pins to be used in maximum throughput mode.

This SPI interface is different from the standard SPI or QSPI interfaces which most microcontrollers are compatible with

  • Is there a recommended microcontroller or a dedicated chip that can bridge this interface to raspberry pi (via USB for example)?
  • Can the QSPI-to-USB mode of FT4222H be used to read data from AD7381-4 in 4-wire mode? How should the schematic connections between the two chips look like?
  • Any other suggestions?

Thank you