Post Go back to editing

LTC2444, LTC2448 analog input pin connection

Category: Hardware
Product Number: LTC2444, LTC2448

Hello,

I'm DFAE. I receuved a question from my customer.

He would like to use LTC2444 or LTC2448 for same PCB and software because of availability issue of them. He use only CH0 channel by single -ended mode. Can we short(connevt) pin 8 and pin 9 of LTC2444 or LTC2448 to achieve that? 

Best regards,

Akira

Top Replies

    •  Analog Employees 
    Aug 18, 2022 in reply to JCCillion +1 verified

    Hi ,

    I have confirmed with the design team that it is possible to short pin 8 and 9 together on both the LTC2444 and LTC2448 for single-ended CH0 measurement (CH0 to COM). Those pins are not internally…

Parents Reply Children