Post Go back to editing

MAX22000 Analog I/O linux options

Category: Software
Product Number: MAX22000

Hi there,

I was hoping to use the MAX 22000 with my current device in the hopes of measuring the current and voltage of a connected Medium-High voltage device.

I have purchased the eval board and have conducted testing using a windows PC, but the device it will be connected to has a Linux(ubuntu) OS and I was hoping to use the device with said device. I realize that the MAX22000 is not compatible with Linux(unless I am mistaken), so I was wondering if it were possible to have access to the source code (for the MAX22000 application).

If it is not possible and I was wondering if you could advise an alternative Analog I/O that can measure both current and Voltage and is compatible with Linux.

Thank you very much,

Tayeb

Parents Reply Children
No Data