Post Go back to editing

MAX22000 Analog I/O linux options

Category: Software
Product Number: MAX22000

Hi there,

I was hoping to use the MAX 22000 with my current device in the hopes of measuring the current and voltage of a connected Medium-High voltage device.

I have purchased the eval board and have conducted testing using a windows PC, but the device it will be connected to has a Linux(ubuntu) OS and I was hoping to use the device with said device. I realize that the MAX22000 is not compatible with Linux(unless I am mistaken), so I was wondering if it were possible to have access to the source code (for the MAX22000 application).

If it is not possible and I was wondering if you could advise an alternative Analog I/O that can measure both current and Voltage and is compatible with Linux.

Thank you very much,

Tayeb

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.