Post Go back to editing

Cannot load COM Module

Thread Summary

The user encountered a 'Cannot load COM module' error when installing a driver for a demo board using QuikEval. The final answer provides a table listing the part numbers, DC board numbers, class IDs, and URLs for the relevant COM module installers. The solution involves downloading the appropriate installer from the provided URL and running it to make the software available in the Linear Technology folder from the Windows Start menu.
AI Generated Content
Category: Software
Product Number: DC590, DC2026, QuikEval

If you receive a Cannot load COM module error message when trying to install a driver for a demo board using QuikEval, the following locations can be used to manually install the COM module. After downloadding the module, run the installer and the software will be available from the Windows Start menu iside the Linear Technology folder.

Part Number DC Board Number Class ID Url
ADL5920 EvalADL5920 D5596 ltspice.analog.com/.../ins5596.msi
LT3964 DC2424A D3964 ltspice.analog.com/.../ins3964.msi
LTC1660 DC2795A-A D1661 ltspice.analog.com/.../ins1661.msi
LTC1661 DC2789A-A D1661 ltspice.analog.com/.../ins1661.msi
LTC1662 DC2789A-B D1661 ltspice.analog.com/.../ins1661.msi
LTC1664 DC2795A-C D1661 ltspice.analog.com/.../ins1661.msi
LTC1665 DC2795A-B D1661 ltspice.analog.com/.../ins1661.msi
LTC2310-12 DC1563A-E D2315 ltspice.analog.com/.../ins2315.msi
LTC2310-12 DC2425A-F D2315 ltspice.analog.com/.../ins2315.msi
LTC2310-14 DC1563A-J D2315 ltspice.analog.com/.../ins2315.msi
LTC2310-14 DC2425A-D D2315 ltspice.analog.com/.../ins2315.msi
LTC2310-16 DC2425A-B D2315 ltspice.analog.com/.../ins2315.msi
LTC2311-12 DC1563A-D D2315 ltspice.analog.com/.../ins2315.msi
LTC2311-12 DC2425A-E D2315 ltspice.analog.com/.../ins2315.msi
LTC2311-14 DC1563A-I D2315 ltspice.analog.com/.../ins2315.msi
LTC2311-14 DC2425A-C D2315 ltspice.analog.com/.../ins2315.msi
LTC2311-16 DC2425A-A D2315 ltspice.analog.com/.../ins2315.msi
LTC2312-12 DC1563A-C D2315 ltspice.analog.com/.../ins2315.msi
LTC2312-14 DC1563A-H D2315 ltspice.analog.com/.../ins2315.msi
LTC2313-12 DC1563A-B D2315 ltspice.analog.com/.../ins2315.msi
LTC2313-14 DC1563A-G D2315 ltspice.analog.com/.../ins2315.msi
LTC2314 DC1563A-F D2315 ltspice.analog.com/.../ins2315.msi
LTC2315 DC1563A-A D2315 ltspice.analog.com/.../ins2315.msi
LTC2320-12 DC2395A-G D2374 ltspice.analog.com/.../ins2374.msi
LTC2320-14 DC2395A-D D2374 ltspice.analog.com/.../ins2374.msi
LTC2320-16 DC2395A-A D2374 ltspice.analog.com/.../ins2374.msi
LTC2321-12 DC1996A-F D2315 ltspice.analog.com/.../ins2315.msi
LTC2321-14 DC1996A-D D2315 ltspice.analog.com/.../ins2315.msi
LTC2321-16 DC1996A-B D2315 ltspice.analog.com/.../ins2315.msi
LTC2323-12 DC1996A-E D2315 ltspice.analog.com/.../ins2315.msi
LTC2323-14 DC1996A-C D2315 ltspice.analog.com/.../ins2315.msi
LTC2323-16 DC1996A-A D2315 ltspice.analog.com/.../ins2315.msi
LTC2324-12 DC2395A-H D2374 ltspice.analog.com/.../ins2374.msi
LTC2324-14 DC2395A-E D2374 ltspice.analog.com/.../ins2374.msi
LTC2324-16 DC2395A-B D2374 ltspice.analog.com/.../ins2374.msi
LTC2325-13 DC2395A-I D2374 ltspice.analog.com/.../ins2374.msi
LTC2325-15 DC2395A-F D2374 ltspice.analog.com/.../ins2374.msi
LTC2325-16 DC2395A-C D2374 ltspice.analog.com/.../ins2374.msi
LTC2326-16 DC1908A-I D2315 ltspice.analog.com/.../ins2315.msi
LTC2326-18 DC1908A-F D2315 ltspice.analog.com/.../ins2315.msi
LTC2327-16 DC1908A-H D2315 ltspice.analog.com/.../ins2315.msi
LTC2327-18 DC1908A-E D2315 ltspice.analog.com/.../ins2315.msi
LTC2328-16 DC1908A-G D2315 ltspice.analog.com/.../ins2315.msi
LTC2328-18 DC1908A-D D2315 ltspice.analog.com/.../ins2315.msi
LTC2328-18 DC2405A-A D2315 ltspice.analog.com/.../ins2315.msi
LTC2333-16 DC2365A-H D2374 ltspice.analog.com/.../ins2374.msi
LTC2333-18 DC2365A-D D2374 ltspice.analog.com/.../ins2374.msi
LTC2335-16 DC2412A-B D2374 ltspice.analog.com/.../ins2374.msi
LTC2335-18 DC2412A-A D2374 ltspice.analog.com/.../ins2374.msi
LTC2336 DC1908A-C D2315 ltspice.analog.com/.../ins2315.msi
LTC2337 DC1908A-B D2315 ltspice.analog.com/.../ins2315.msi
LTC2338 DC1908A-A D2315 ltspice.analog.com/.../ins2315.msi
LTC2341-16 DC2581A-B D2374 ltspice.analog.com/.../ins2374.msi
LTC2341-18 DC2581A-A D2374 ltspice.analog.com/.../ins2374.msi
LTC2343-16 DC2094A-F D2374 ltspice.analog.com/.../ins2374.msi
LTC2343-18 DC2094A-C D2374 ltspice.analog.com/.../ins2374.msi
LTC2344-16 DC2520A-B D2374 ltspice.analog.com/.../ins2374.msi
LTC2344-18 DC2520A-A D2374 ltspice.analog.com/.../ins2374.msi
LTC2345-16 DC2326A-B D2374 ltspice.analog.com/.../ins2374.msi
LTC2345-18 DC2326A-A D2374 ltspice.analog.com/.../ins2374.msi
LTC2347-16 DC2094A-E D2374 ltspice.analog.com/.../ins2374.msi
LTC2347-18 DC2094A-B D2374 ltspice.analog.com/.../ins2374.msi
LTC2348-16 DC2094A-D D2374 https://ltspice.analog.com/quikeval/ins2374.msi
LTC2348-18 DC2094A-A D2374 ltspice.analog.com/.../ins2374.msi
LTC2353-16 DC2365A-G D2374 ltspice.analog.com/.../ins2374.msi
LTC2353-18 DC2365A-C D2374 ltspice.analog.com/.../ins2374.msi
LTC2357-16 DC2365A-F D2374 ltspice.analog.com/.../ins2374.msi
LTC2357-18 DC2365A-B D2374 ltspice.analog.com/.../ins2374.msi
LTC2358-16 DC2365A-E D2374 ltspice.analog.com/.../ins2374.msi
LTC2358-18 DC2365A-A D2374 ltspice.analog.com/.../ins2374.msi
LTC2368-24 DC2289A-B D2374 ltspice.analog.com/.../ins2374.msi
LTC2372-16 DC2071A-E D2374 ltspice.analog.com/.../ins2374.msi
LTC2372-18 DC2071A-B D2374 ltspice.analog.com/.../ins2374.msi
LTC2373-16 DC2071A-D D2374 ltspice.analog.com/.../ins2374.msi
LTC2373-18 DC2071A-A D2374 ltspice.analog.com/.../ins2374.msi
LTC2374-16 DC2071A-C D2374 ltspice.analog.com/.../ins2374.msi
LTC2376-20 DC1925A-C D2315 ltspice.analog.com/.../ins2315.msi
LTC2377-20 DC1925A-B D2315 ltspice.analog.com/.../ins2315.msi
LTC2378-20 DC1925A-A D2315 ltspice.analog.com/.../ins2315.msi
LTC2378-20 DC2135A D2315 ltspice.analog.com/.../ins2315.msi
LTC2380-24 DC2289A-A D2374 ltspice.analog.com/.../ins2374.msi
LTC2449 DC1410B D2449 ltspice.analog.com/.../ins2449.msi
LTC2498 DC1410A D2449 ltspice.analog.com/.../ins2449.msi
LTC2500-32 DC2222A-A D2374 ltspice.analog.com/.../ins2374.msi
LTC2508-32 DC2222A-B D2374 ltspice.analog.com/.../ins2374.msi
LTC2512-24 DC2222A-C D2374 ltspice.analog.com/.../ins2374.msi
LTC2662-12 DC2692A-B D2662 ltspice.analog.com/.../ins2662.msi
LTC2662-16 DC2692A-A D2662 ltspice.analog.com/.../ins2662.msi
LTC2664-12 DC2376A-B D2668 ltspice.analog.com/.../ins2668.msi
LTC2664-16 DC2376A-A D2668 ltspice.analog.com/.../ins2668.msi
LTC2666-12 DC2196A-B D2668 ltspice.analog.com/.../ins2668.msi
LTC2666-16 DC2196A-A D2668 ltspice.analog.com/.../ins2668.msi
LTC2668-12 DC2025A-B D2668 ltspice.analog.com/.../ins2668.msi
LTC2668-16 DC2025A-A D2668 ltspice.analog.com/.../ins2668.msi
LTC2672-12 DC2903A-B D2662 ltspice.analog.com/.../ins2662.msi
LTC2672-16 DC2903A-A D2662 ltspice.analog.com/.../ins2662.msi
LTC2874 DC1880A D2874 ltspice.analog.com/.../ins2874.msi
LTC2943 DC1812A-A D2943 ltspice.analog.com/.../ins2943.msi
LTC2943-1 DC1812A-C D2943 ltspice.analog.com/.../ins2943.msi
LTC2944 DC1812A-B D2943 ltspice.analog.com/.../ins2943.msi
LTC2947 DC2334A D2947 ltspice.analog.com/.../ins2947.msi
LTC2947-65 DC2826A D2947-65 ltspice.analog.com/.../ins2947-65.msi
LTC2949 DC2732A-A D2949 ltspice.analog.com/.../ins2949.msi
LTC2949 DC2732A-B D2949 ltspice.analog.com/.../ins2949.msi
LTC2949 DC2732A-C D2949 ltspice.analog.com/.../ins2949.msi
LTC2983 DC2209A D2983 ltspice.analog.com/.../ins2983.msi
LTC2984 DC2399A D2984 ltspice.analog.com/.../ins2984.msi
LTC2986 DC2508A D2986 ltspice.analog.com/.../ins2986.msi
LTC2986-1 DC2618A D2986-1 ltspice.analog.com/.../ins2986-1.msi
LTC2991 DC1785A D2991 ltspice.analog.com/.../ins2991.msi
LTC2992 DC2561A D2992 ltspice.analog.com/.../ins2992.msi
LTC3300-1 DC2064A D33001 ltspice.analog.com/.../em33001.exe
LTC3350 DC1937 D3350 ltspice.analog.com/.../ins3350.msi
LTC3351 DC2464AA D3351 ltspice.analog.com/.../ins3351.msi
LTC3351 DC2464AB D3351 ltspice.analog.com/.../ins3351.msi
LTC3375 DC1921 D3375 ltspice.analog.com/.../ins3375.msi
LTC3589 DC1558A D3589 ltspice.analog.com/.../ins3589.msi
LTC3589-1 DC1808A D35891 ltspice.analog.com/.../ins35891.msi
LTC3589-1 DC1808B-A D35891 ltspice.analog.com/.../ins35891.msi
LTC3589-2 DC1808B-B- D35892 ltspice.analog.com/.../ins35892.msi
LTC3676 DC1976A-A D3676 ltspice.analog.com/.../ins3676.msi
LTC3676-1 DC1976A-B D36761 ltspice.analog.com/.../ins36761.msi
LTC4155 DC1674A-A D4155 ltspice.analog.com/.../ins4155.msi
LTC4156 DC1674A-B D4156 ltspice.analog.com/.../ins4156.msi
LTC4261 DC998A D4261 ltspice.analog.com/.../ins4261.msi
LTC4266 DC1366 D4266 ltspice.analog.com/.../em4266.exe
LTC4266 DC1815 D4266 ltspice.analog.com/.../em4266.exe
LTC4271 DC1679 D4271 ltspice.analog.com/.../em4271.exe
LTC4271 DC1680 D4271 ltspice.analog.com/.../em4271.exe
LTC4271 DC1843 D4271 ltspice.analog.com/.../em4271.exe
LTC4291 DC2685 D4291 ltspice.analog.com/.../ins4291.msi
LTC4316 DC2217A D4316 ltspice.analog.com/.../ins4316.msi
LTC5586 DC2349A D5586 ltspice.analog.com/.../ins5586.msi
LTC5589 DC2391A-A D5599 ltspice.analog.com/.../ins5599.msi
LTC5594 DC2645A D5594 ltspice.analog.com/.../ins5594.msi
LTC5596 EvalLTC5596 D5596 ltspice.analog.com/.../ins5596.msi
LTC5597 DC3128A D5596 ltspice.analog.com/.../ins5596.msi
LTC5599 DC2091A D5599 ltspice.analog.com/.../ins5599.msi
LTC6802 DC1331A D6802 ltspice.analog.com/.../em6802.exe
LTC6802-2 DC1393A D6802-2 ltspice.analog.com/.../em6802-2.exe
LTC6803-1 DC1651A D6803-1 ltspice.analog.com/.../em6803-1.exe
LTC6803-2 DC1652A D6803-2 ltspice.analog.com/.../em6803-2.exe
LTC6803-3 DC1653A D6803-3 ltspice.analog.com/.../em6803-3.exe
LTC6803-4 DC1654A D6803-4 ltspice.analog.com/.../em6803-4.exe
LTC6804-1 DC1894A D6804-1 ltspice.analog.com/.../ins6804-1.msi
LTC6804-2  DC1942A D6804-2 ltspice.analog.com/.../ins6804-2.msi
LTC6811-1 DC2259A D6811-1 ltspice.analog.com/.../ins6811-1.msi
LTC6811-2 DC2260A D6811-2 ltspice.analog.com/.../ins6811-2.msi
LTC6945 DC1649A-A D6945 ltspice.analog.com/.../n20m6945.msi
LTC6946-1 DC1705B-A D6945 ltspice.analog.com/.../n20m6945.msi
LTC6946-1 DC1705C-A D6945 ltspice.analog.com/.../n20m6945.msi
LTC6946-2 DC1705B-B D6945 ltspice.analog.com/.../n20m6945.msi
LTC6946-3 DC1705B-C D6945 ltspice.analog.com/.../n20m6945.msi
LTC6946-3 DC1705C-C D6945 ltspice.analog.com/.../n20m6945.msi
LTC6946-4 DC1705C-D D6945 ltspice.analog.com/.../n20m6945.msi
LTC6947 DC1846A D6947 ltspice.analog.com/.../ins6947.msi
LTC6948-1 DC1959B-A D6947 ltspice.analog.com/.../ins6947.msi
LTC6948-2 DC1959B-B D6947 ltspice.analog.com/.../ins6947.msi
LTC6948-3 DC1959B-C D6947 ltspice.analog.com/.../ins6947.msi
LTC6948-4 DC1959B-D D6947 ltspice.analog.com/.../ins6947.msi
LTC6948-4 DC2030A-D D6947 ltspice.analog.com/.../ins6947.msi
LTC6950 DC1795A D6950 ltspice.analog.com/.../ins6950.msi
LTC6952 DC2609A D6952 ltspice.analog.com/.../ins6952.exe
LTC6953 DC2610A D6952 ltspice.analog.com/.../ins6952.exe
LTC6954-1 DC1954A-A D6954 ltspice.analog.com/.../ins6954.msi
LTC6954-2 DC1954A-B D6954 ltspice.analog.com/.../ins6954.msi
LTC6954-3 DC1954A-C D6954 ltspice.analog.com/.../ins6954.msi
LTC6954-4 DC1954A-D D6954 ltspice.analog.com/.../ins6954.msi
LTC7871 DC2886A D7871 ltspice.analog.com/.../ins7871.msi
LTC7872 DC3038A D7872 ltspice.analog.com/.../ins7872.msi
LTM2895 DC2589A D2895 ltspice.analog.com/.../ins2895.msi
LTM2985 DC2872A D2985 ltspice.analog.com/.../ins2985.msi
LTM9100 DC2423A-A D4261 ltspice.analog.com/.../ins4261.msi
LTM9100 DC2423A-B D4261 ltspice.analog.com/.../ins4261.msi