Post Go back to editing

DC590B & DC2094A Msg : Cannot load COM module for the device

Category: Software
Product Number: DC2094A-D

I installed successfully the QuikEval software and drivers for the DC590B Controller. The connected DC590B with the LTC2348-16 was detected by the QuikEval Software. After pressing the button "Open" I get the message "Cannot load COM module for the device". Is there a link where I can download the required software driver for the LTC2348-16?

Thank you in advance.

Top Replies

Parents
  • What is written in the EEPROM in the DC1812A-B module? If I use the LTC2944 directly as a product, I want to connect QUILEVAL or the LTC2944MSI software directly, without this EEPROM, is it possible?

    In fact, without the EEPROM on the DC1812 module, the two upper computer software cannot be opened, and the display shows LTC Devices not found, which is a very strange phenomenon.

Reply
  • What is written in the EEPROM in the DC1812A-B module? If I use the LTC2944 directly as a product, I want to connect QUILEVAL or the LTC2944MSI software directly, without this EEPROM, is it possible?

    In fact, without the EEPROM on the DC1812 module, the two upper computer software cannot be opened, and the display shows LTC Devices not found, which is a very strange phenomenon.

Children