Post Go back to editing

DC590B & DC2094A Msg : Cannot load COM module for the device

Thread Summary

The user encountered a 'Cannot load COM module for the device' error when trying to open the LTC2348-16 with the DC590B Controller in QuikEval software. The solution is to download and install the specific software driver from the provided link. The driver can be accessed from the Start menu in the Linear Technology folder after installation.
AI Generated Content
Category: Software
Product Number: DC2094A-D

I installed successfully the QuikEval software and drivers for the DC590B Controller. The connected DC590B with the LTC2348-16 was detected by the QuikEval Software. After pressing the button "Open" I get the message "Cannot load COM module for the device". Is there a link where I can download the required software driver for the LTC2348-16?

Thank you in advance.