Post Go back to editing

AD7771 Phase Adjustment Question

Thread Summary

The user is experiencing issues with phase adjustment on the AD7771 ADC when setting different CHx_SYNC_OFFSET values. The final answer suggests setting the channel with the largest phase delay (CH1 in this case) to 0, and adjusting the other channels relative to it. The decimation rate is 32, and the phase delay must be less than this value. The user confirms that setting CH3 to 0 and adjusting other channels works, but Ia and Ic only function correctly with 0 or 31.
AI Generated Content
Category: Software
Product Number: AD7771
Software Version: CCES

Hi everyone, 

I am new in DSP. I have a problem when programming the AD7771. 

I was trying to use phase adjustment for each ADC. However, the function only works when I set all CHx_SYNC_OFFSET with same number, other wise only smallest one work. 

for example: my Decimation Rate = 32. 

                     the function will work for all ADC if i make CH(0-7)_SYNC_OFFSET = 17(0x11); 

                     if I set eg: CH(3)_SYNC_OFFSET = 16 and maintain rest of them equal to 17. Only CH3 will do phase adjustment. However, when i check the data in each channels they give me correct data which means I have successfully wrote the data to each registers. 

I also have hard time to understand "Phase Adjustment" part in Data Sheet. 

                . "In other words, programming the channel with higher phase delay as CHx_SYNC_OFFSET= 0, any other channel with lower phase, can be delayed to compensate for the phase mismatch."[p.42]

I am not sure is this the reason only smaller number in register can work? 

 

best regards,

Bolin                  

Parents
  • Hi Bolin,

    If you write the same number to all the SYNC_OFFSET you will see the same phase delay in all the signals so the effect will be like doing nothing.

    The phase delay must be relative to the at least one channel (normally the one with has highest phase delay since it is the slowest). This channel must be configured with 0x0 phase delay and all the others will take that channel as a reference for their delays.

    As it is specified in the datasheet, the phase delay must always be lower than the decimation rate.

    I would recommend to set to 0 the channel with highest phase delay, play around with the value of SYNC_OFFSET of the other and plot the data to see if there is any change when the SYN_OFFSET is change.

    Regards

    Joan

  • Thanks Joan, 

    I should give more information about my case, I am working on Three phase power system. CH0-3 is current A to C and N, CH 4-6 is voltage. the data shows that CH1 which is Ib has largest phase delay. So I set CH3 = 0. I can change Va-Vc (Ch4-6) to any number and it gives me expected result. however, Ia and Ic can only be set to 0 or 31 other wise the output data will be wrong.

    hope I describe clearly. 

    Best regards,

    Bolin

Reply
  • Thanks Joan, 

    I should give more information about my case, I am working on Three phase power system. CH0-3 is current A to C and N, CH 4-6 is voltage. the data shows that CH1 which is Ib has largest phase delay. So I set CH3 = 0. I can change Va-Vc (Ch4-6) to any number and it gives me expected result. however, Ia and Ic can only be set to 0 or 31 other wise the output data will be wrong.

    hope I describe clearly. 

    Best regards,

    Bolin

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.