Post Go back to editing

Default filtering in Zedboard + AD4630

Category: Software
Product Number: AD4630-24 + Zedboard

Hi,

I've recently purchased Zedboard + Eval-AD4630. The thing is that the ADC is 2MSps but I see the bandwidth is below 30kHz. As long as I sweep a sine signal I see a huge reduction in the acquisition above 20kHz when it should behave like this. Aby idea if it is teh board or the ADC? Isee nothing in the specs of both.

Regards