Post Go back to editing

AD5940 SensorPal firmware source code

Category: Software
Product Number: SensorPal
Software Version: 2525

Hello,

I would like to know if Sensor PAL AD5940 firmware source code is it available somewhere. I could check that inside SensorPal installation path there is only a firmware binary file but there is no mention to source code.

I am working with https://github.com/analogdevicesinc/ad5940-examples source code to create my app, but using SensorPal to get information from sensor kit. I want the SensorPal firmware to be configured the same as the github code above in order to get same results.

Regards

Parents
  • Hi,

    1. Do you want the SensorPal GUI firmware source code to be provided to you?  
      1. If yes, we cannot provide the SensorPal GUI Firmware due to the licensing.
    2. I want the SensorPal firmware to be configured the same as the github code above in order to get same results., what specific technique(s) are you using/testing?
    3. Is it that you are getting the correct data in example firmware and you want to get the same data in SensorPal GUI? If yes, what measurement technique?
  • Hello,

    Yes, your third point is what I am trying to do. I want to be sure that the firmware source code in github repository is configured the same way as the SensorPal GUI software.

    The measurement techniques I want to use are Body Impedance and Electrodermal Activity.

    I know that you can check different settings in the SensorPal GUI, and these values can be compared to the values provided by github firmware examples. It is just to make sure that both, the SensorPal GUI and the GitHub firmware examples, are configured the same way.

    I talked about the SensorPal firmware source code so I can check its default settings, but if you can not provide it, I understand.

    Regards

Reply
  • Hello,

    Yes, your third point is what I am trying to do. I want to be sure that the firmware source code in github repository is configured the same way as the SensorPal GUI software.

    The measurement techniques I want to use are Body Impedance and Electrodermal Activity.

    I know that you can check different settings in the SensorPal GUI, and these values can be compared to the values provided by github firmware examples. It is just to make sure that both, the SensorPal GUI and the GitHub firmware examples, are configured the same way.

    I talked about the SensorPal firmware source code so I can check its default settings, but if you can not provide it, I understand.

    Regards

Children
No Data