Post Go back to editing

AD7741 not working

Category: Hardware
Product Number: AD7741

Hi,

I have been trying to make a board work with the AD7741 I have used the schematic of the development board as a reference but it is not working and I have no idea what else can it be or if the chip actually got fried in a test. I am using a crystal oscillator of 400 kHz which is oscillating fine and also I can see the oscillation on the CLKOUT pin of the 7741 but I can't see any frequency coming out on the Fout pin I am not sure what is the issue I hope someone has an schematic or guide which they had used for this specific device.

Cheers,

Marfil