Post Go back to editing

AD4030-24 in Single-Ended Mode?

Category: Hardware
Product Number: AD4030-24

Hello,

i want to use the new AD4030-24 24-Bit ADC in a Single-Ended Input configuration, to digitize a 0V to 5V signal.

Unfortunately the Datasheet only says that it it possible to use the device in a Single-Ended configuration, but it does not tell how to do it properly.

Is it possible to just ground the negativ input pin with losing one bit of resolution, or is there a better way?

As the reference voltage I would use the recommended AD4550 (5V).

Best regards,

Dennis