The AD598 datasheet specify a drive distance over a cable of 300 feet.
There are no informations in the AD698 on how much cable length can be driven.
Thanks
AD698
Production
The AD698 is a complete, monolithic Linear Variable Differential Transformer (LVDT) signal conditioning subsystem. It is used in conjunction with LVDTs...
Datasheet
AD698 on Analog.com
AD598
Production
The AD598 is a complete, monolithic Linear Variable Differential Transformer (LVDT) signal conditioning subsystem. It is used in conjunction with LVDTs...
Datasheet
AD598 on Analog.com
The AD598 datasheet specify a drive distance over a cable of 300 feet.
There are no informations in the AD698 on how much cable length can be driven.
Thanks
Hi,
The AD698 has the ability to drive a longer cable length compared to the AD598 since it has a higher output voltage and excitation current. Note that both LVDT Signal conditioner does not require a constant amplitude because it works on the ratio of the difference and sum of the LVDT output signals.
Regards,
Andrei