This Product Change Notification dated Feb. 2022 show that they are similar
This Product Change Notification dated Feb. 2022 show that they are similar
Hi,
Apologies, I don't think this is available for open market. May I know what is your application? Is the reason for the replacement is due to no stocks issues? Are you open for other part replacement or does it need to be pin-pin compatible?
Thanks,
Jellenie
It's a no stock issue. I'm trying to find something that is preferably pin compatible. But would consider same specs with different pinout. Can I get the datasheet for AD70041Z-0U1 ? I may try to figure it out myself.
Application is operating temperature critical: -40oC to +125oC. But I'm willing to consider a narrower operating range if pin compatible.
Application is operating temperature critical: -40oC to +125oC. But I'm willing to consider a narrower operating range if pin compatible.
Hi,
We have a newly released ADC AD4130-8 Datasheet and Product Info | Analog Devices which has most of the building blocks of AD7124-8 with a much lower consumption but with similar performance with AD7124-8 at low power mode. It also have extra feature for system level power savings such as FIFO. Though the package of this part is WLCSP and the temperature range is up to 105'C only.
May I know what is your specific applications and what AD7124-8 features do you require for this application so I can recommend other options.
Thanks,
Jellenie
Which chip is at least pin compatible with AD70041Z-0U1 ? AD7124-8 or AD4130-8 ?
Could you send me the link to datasheet of AD70041Z ? So I can make my mind myself about any substitute.
Hi
Apologies. I cannot disclose any information about the above part in this thread as like I have mentioned this is not for public or open market.
I would recommend to contact your local FAE to discuss this offline.
Thanks,
Jellenie