Post Go back to editing

AD7124 relationship between absolute maximum voltage and absolute maximum current

Hi,

I am considering AD7124-4.

I saw the absolute maximum rating of AD7124.
"Analog Input Voltage to AVss" is "-0.3V to A VDD + 0.3V".
"AINx / Digital Input Current" is "10mA".

If I protect the AINx from a current of 10mA or more, is it okay if a voltage of  AVDD + 0.3V or more is applied to the AINx?

Best regards,

Yuya