when I type the 0x80 data into the interface register, that is, when I set the "contread" bit, I see that all register values get 0xFFFF or irrelevant values. however, I did not forget to configure it in the continuous conversion mode to use the continuous reading mode.everything is normal before writing 0x80 to the interface register.
is there a special case that needs to be known when configuring the interface record or writing to this record?
so far, I have made healthy measurements for various configuration settings related to other recording settings. in general, I figured out how to use " AD4111". but I have a problem with only the "contrread" bit of the interface register.