Post Go back to editing

Continuous Sampling Capability of EVAL-AD4134 using ACE

Thread Summary

The user inquired about using the EVAL-AD4134 with the SDP-H1 and ACE software to sample three differential input channels at 200kHz for 10 seconds. The final answer confirmed that the SDP-H1 card cannot store 2M samples, with a maximum of 131k samples. The EVAL-AD4134's 'Run Continuous Mode' in ACE software was mentioned, but its limitations for this specific application were noted.
AI Generated Content

Hello everyone

I would like to evaluate the AD4134 in an application in which I need to measure the third harmonic of a 30kHz fundamental frequency signal for three pickup coils. I would like to use the EVAL-AD4134 for this purpose.

I would like to sample three differential input channels for a period of around 10 seconds with a sampling rate of at least 200kHz.

Is it possible to do this with the EVAL-AD4134 / SDP-H1 and the ACE software?

(The documentation of the EVAL-AD4134 mentions a "Run Continuous Mode" for data acquisition in the ACE software but I am not sure if there are any limitations here on the number of channels or sampling rates)?

Thanks!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.