AD2S1210
Production
The AD2S1210 is a complete 10-bit to 16-bit resolution tracking resolver-to-digital converter, integrating an on-board programmable sinusoidal oscillator...
Datasheet
AD2S1210 on Analog.com
Hello everyone.
I have used te AD2S1210 in several projects along with a common 6 wire resolver (EXHI, EXLO, SIN, SINLO, COS, COSLO) without any problem using the excitation buffer suggested in the datasheet and the following input stage with the appropiate optional values to meet the input range of the IC.
However, now i have to work with a 5 wire resolver, where SINLO and COSLO are tied together internally, i have tried to use the same approach but is not working at all, randomly activating multiple error flags in the fault register (LOT, DOS mismatch threshold and other bit i do not remember). Here you have a LTSpice capture of the actual circuit i am trying to use:
Analyzing signal received by the ADS1210 when, for exampe, SINE is maximum, COSINE is still showing few millivolts differentially, and a sinusodial voltage is present in COS/COSLO pins, here you can see the effect, from top to bottom, excittion (4 Vrms), IC COS input differential, IC COS and COSLO inputs respect GND, IC SIN input differential, IC SIn and SINLO inputs respect GND)
Removing the connection between SINLO and COSLO gets rid of this effect.
May the connection between SINLO and COSLO causing the problem with the error flags? If so, how can i solve this issue?
Thanks in advance.
manuslet,
This sounds suspiciously like you are using a synchro as your sensor. Can you please share the part # for the sensor so that I can do a bit of research to confirm.
If this is the case you can use a Scott-T transformer to convert the 3-Phase output of the sensor into a 2-Phase quadrature signal you'll need to drive the AD2S1210 and that should eliminate your problem assuming you adhere to the input parametric specifications in the datasheet.
Sean
manuslet,
There is an application note for the AD2S80 (AN-252) published some time ago that shows how to convert the stator signals using op-amps to create single-ended inputs needed for that product family. I would argue you could use the same principles and a dual fully differential amplifier to accomplish the same function. The reason I mention this is a quick search for Scott-T transformers only produced very large power conversion offerings which I'm sure are significantly over specified for your application. This solid state solution may be just what you need.
Sean
manuslet,
There is an application note for the AD2S80 (AN-252) published some time ago that shows how to convert the stator signals using op-amps to create single-ended inputs needed for that product family. I would argue you could use the same principles and a dual fully differential amplifier to accomplish the same function. The reason I mention this is a quick search for Scott-T transformers only produced very large power conversion offerings which I'm sure are significantly over specified for your application. This solid state solution may be just what you need.
Sean