Post Go back to editing

AD4003 negative output

Thread Summary

The user is experiencing sign reversal in the ADC output when using the AD4003 in 3-wire turbo mode with a 100 MHz clock and a 3V differential input signal. The issue is due to the common mode input voltage being out of spec (1.5V instead of 2.5V for a 5V VREF). The solution involves using a fully differential amplifier like the ADA4940 or ADA4945 to meet the common mode input voltage requirement, or switching to the single-ended AD4002.
AI Generated Content

Hi,

I am using AD4003 ADC in one of the design. In this we are using 3-wire turbo mode.

Clock frequency used is 100Mhz.

Now when I provide 3V differential signal to the input of ADC. I am getting a hex value 0x2D0CD which is near to -3V(Read on SDO line).

My question is why I am getting output of ADC with sign reversal?

Regards,

Rohit