Hey there,
i'm interested to use LTC2480. I also like to use his internal Temperature Sensor. But i can't find anything about the accuray of the internal temperature sensor. Can someone provide a Graph over Temperature and multiple LTC2480 to see how accurate the LTC2480 is?
Only thing i found in Datasheet is at Page 3 Internal PTAT Signal 390-450mV with typical Value of 420mV+-30mV. Gradient is 1.4mV/C... That means: 27°C +-21.4286°C isn't it?
Cheers!