Post Go back to editing

AD4115 with switched power-supplies

Hi, I want to use the AD4115 with switched power-supplies. Do they have negative impact on accuracy?

The application is a Battery Management System (BMS), sampling every second voltage, amperes and temperatures. During main of that second, the current used b the BMS should be at low as possible. A switched power-supply  (i.e. MAX25232 or LM33630, or a AD alternative not searched for yet) can operate in High Efficiency with low load.

The most accuracy needed is measurings amps during charge or load, from some mA up to 200A.

Parents Reply
  • Hi, 

    We do not usually recommend to supply switching regulator directly to our ADCs that is why Andrei is recommending to add an additional external series LDO. I think a switching regulator is okay if you have a proper isolation, so an additional extra power isolation can also be an option.  

    Thanks,

    Jellenie 

Children